When should I use the sticky pads provided instead of the screws when installing my sensor?

If the surface where you wish to mount the door and window sensors or motion sensors is smooth, i.e. UPVC, wood or painted wall, it is recommended to fit these devices without tools, using the sticky pads provided. Ensure the surface is clean before sticking in position. The sticky pad will provide optimum strength after 24 hours.