I have a Honeywell Quick Start Alarm Kit (siren-based). Why doesn’t the wireless door and window sensor trigger the alarm?

Try one of the following solutions in this order:

  1. Ensure that the sensor is within effective radio range of the Siren and is not mounted close to metal objects which may interfere with the wireless radio transmission.
  2. Ensure the battery isolation tab has been removed from the side of the sensor.

    ka_linking_new_magnetic_door_window_sensor_5

  3. Ensure that the gap between the Magnet and Sensor is no more than than 10mm.

    ka_positioning_the_door_window_sensor_4

  4. Check and replace the battery in the door and window sensor.

    If the above does not work, you will need to re-link the wireless door and window sensor to the Siren. Check the relevant FAQ or the Instruction Manual on how to do this.