I have a Honeywell Quick Start Alarm Kit (Siren-based alarm). The Siren has power (flashing LEDs) but will not respond to the remote control. How do I fix this?

The Siren could be in Service mode. Switch the Siren to Operating Mode:

  1. Press and hold the ‘Disarm’ button ka_disarm on your remote control key fob for 5 seconds.
  2. The siren should produce a single long beep followed 1 second later by two short beeps.

    bss_beeeeeep_beep

  3. The Siren LEDs will flash together in conjunction with the beeps.
  4. If the Siren still does not respond, check to see if the Remote Control or Siren batteries are low. Otherwise, the remote control may need to be re-linked to the Siren.