How do I link a Honeywell wireless doorbell to my Honeywell alarm keypad to enable the doorbell as an additional intenal siren?

  1. Enter Programming mode by pressing the Programme button followed by swiping a contactless tag or entering your PIN code. The keypad will play a melody to indicate success.

    ka_user_pin_code_reset_1 ka_test_mode_2 ka_programming_mode_3

  2. Press and hold the Settings button on your doorbell until an amber light flashes, either from the small LED indicator on the side of the doorbell, or from the Halo Light (depending on product type).

    ka_programming_mode_57

  3. Press the Arm button on the keypad to link it with the doorbell. The doorbell will play a sound.

    ka_programming_mode_58 ka_programming_mode_59

  4. After 30 seconds, the keypad will play a melody. You can now exit programming mode on the keypad by pressing the Programme button again.

    ka_test_mode_7 ka_user_pin_code_reset_1